S32K1 Internal load capacitance in EXTAL and XTAL pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K1 Internal load capacitance in EXTAL and XTAL pin

Jump to solution
940 Views
nxp52415
NXP Employee
NXP Employee

Hello @jesus_sanchez

Apparently the customer needs to fill up a technical sheet for the OEM, and the internal load capacitance that the Quarz crystal sees is required. see datasheet talks about external load capacitance. Could you help me here to explain why we do not provide this value?

Thanks

0 Kudos
1 Solution
922 Views
jesus_sanchez
NXP Employee
NXP Employee

Hi Hector

It is simple. The load capacitance is defined as  "the amount of the external circuit capacitance in parallel with the crystal itself".

In other words. The load capacitance is determined/calculated by external capacitors based on the transconductance of the MCU and the crystal characteristics.

Please check my Hardware Design Guidelines for the S32K1xx

Here the link ---------->

https://nxp1.sharepoint.com/:f:/t/8_8/EjntePi1ypBHqyns4M1xu-oBteOmFVhReS6qTooBUplX0g?e=jr9kef 

 

jesussanchez_1-1616020812103.png

 

 

 

View solution in original post

1 Reply
923 Views
jesus_sanchez
NXP Employee
NXP Employee

Hi Hector

It is simple. The load capacitance is defined as  "the amount of the external circuit capacitance in parallel with the crystal itself".

In other words. The load capacitance is determined/calculated by external capacitors based on the transconductance of the MCU and the crystal characteristics.

Please check my Hardware Design Guidelines for the S32K1xx

Here the link ---------->

https://nxp1.sharepoint.com/:f:/t/8_8/EjntePi1ypBHqyns4M1xu-oBteOmFVhReS6qTooBUplX0g?e=jr9kef 

 

jesussanchez_1-1616020812103.png