S32K1: Data retention of Flash and Emulated EEPROM if at 30C average

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K1: Data retention of Flash and Emulated EEPROM if at 30C average

跳至解决方案
2,490 次查看
john_floros
NXP Employee
NXP Employee

Hello,

Do we have any data on how many years of data retention the Flash and FlexNVM would if the average temperature was at or about 30C.  Could the retention last 50 years?

These question is prompted by Ford requirements:

1. Data retention after 100 erase/write cycles: 50 years (at an average temperature of 30C). 

2. Data retention after 10,000 erase/write cycles: 50 years (at an average temperature of 30C). 

If we do not have the data.  Is it possible to run a simulation or model this to get the data?

Thank you,

John

0 项奖励
回复
1 解答
2,464 次查看
john_floros
NXP Employee
NXP Employee

I will redirect my updates to the following community Link:

Ford - S32K 50years NVM retention - NXP Community

Thank you.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,465 次查看
john_floros
NXP Employee
NXP Employee

I will redirect my updates to the following community Link:

Ford - S32K 50years NVM retention - NXP Community

Thank you.

0 项奖励
回复
2,478 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I have sent you a email directly.

0 项奖励
回复
1,698 次查看
chenhuang
Contributor II

Can you send me a copy of the document?

0 项奖励
回复
1,666 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

There is no document there. There is a discussion on the internal forum, but in the end without any outcome. I would recommend to create new ticket:
https://www.nxp.com/support/support:SUPPORTHOME

 

0 项奖励
回复
1,663 次查看
chenhuang
Contributor II

Ok, thank you very much

0 项奖励
回复