S32K1: Data retention of Flash and Emulated EEPROM if at 30C average

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K1: Data retention of Flash and Emulated EEPROM if at 30C average

Jump to solution
2,411 Views
john_floros
NXP Employee
NXP Employee

Hello,

Do we have any data on how many years of data retention the Flash and FlexNVM would if the average temperature was at or about 30C.  Could the retention last 50 years?

These question is prompted by Ford requirements:

1. Data retention after 100 erase/write cycles: 50 years (at an average temperature of 30C). 

2. Data retention after 10,000 erase/write cycles: 50 years (at an average temperature of 30C). 

If we do not have the data.  Is it possible to run a simulation or model this to get the data?

Thank you,

John

0 Kudos
Reply
1 Solution
2,385 Views
john_floros
NXP Employee
NXP Employee

I will redirect my updates to the following community Link:

Ford - S32K 50years NVM retention - NXP Community

Thank you.

View solution in original post

0 Kudos
Reply
5 Replies
2,386 Views
john_floros
NXP Employee
NXP Employee

I will redirect my updates to the following community Link:

Ford - S32K 50years NVM retention - NXP Community

Thank you.

0 Kudos
Reply
2,399 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I have sent you a email directly.

0 Kudos
Reply
1,619 Views
chenhuang
Contributor II

Can you send me a copy of the document?

0 Kudos
Reply
1,587 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

There is no document there. There is a discussion on the internal forum, but in the end without any outcome. I would recommend to create new ticket:
https://www.nxp.com/support/support:SUPPORTHOME

 

0 Kudos
Reply
1,584 Views
chenhuang
Contributor II

Ok, thank you very much

0 Kudos
Reply