S32K pin in FTM disabled mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K pin in FTM disabled mode

1,055 Views
youssef
Contributor II

Hi all

My question is about FTM module.

I'm looking to know the behavior of S32 FTM pin, if the mux is configured as FTM mode (PORT_PCR_MUX), but the FTM is disabled by (ELSB:ELSBA) in CnSC register.

There is a comment from RM in Table 45-5. Channel Modes Selection, in case of ELSB:ELSA = 00:

"Pin not used for FTM—revert the channel pin to general purpose I/O or other peripheral control"

If the mux of the pin is still configured as FTM mode, what is the behavior ?

Do you have further explanation for this comment?

What is the logic state of the pin in this case? (output Low or high?, input or hi-Z )

Regards

Youssef

Tags (2)
1 Reply

933 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Youssef,

The corresponding digital input buffer (GPIO_PDIR) is active in all digital functions.

If you don't drive the pin externally and the internal pull devices are disabled (PCRn_PE = 0), the pin is floating.

Regards,

Daniel