S32K max supported ISELED

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K max supported ISELED

812 Views
aks029
Contributor I

For POC I will be using S32K-ISELED LED Lighting Solution EVK. 

I want to understand on the  limitations related to

- max number of leds ?

- iseled stack ?

- code size ?

 license for evaluation ?

 

 

0 Kudos
Reply
2 Replies

611 Views
Chaitanyaj
Contributor I

Does S32K144-Q100 includes S32K ISELED part numbers which include the full production license? 

0 Kudos
Reply

788 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @aks029 

The S32K-ISELED Application Development Kit (ADK) comes with a 16-LED bar, but the ISELED Communication Protocol can address up to 4079 LEDs.

The development kit and the non-ISELED S32K standard part number device can only be used with the the free-of-charge evaluation version of the ISELED software driver.

NOTE: Limited functionality: Mandatory driver re-initialization after 150,000 (SDK version) or 10,000 (AUTOSAR version) ISELED commands.

For production, developers should order one of the S32K ISELED part numbers which include the full production license with unlimited driver functionality. 

For more information, please contact ISELED directly or your NXP representative.

 

BR, VaneB

0 Kudos
Reply