S32K how to use the Flexio Shifter operation about Match Store Mode and Match Continuous Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K how to use the Flexio Shifter operation about Match Store Mode and Match Continuous Mode

723 Views
584914019
Contributor III


I want to use FLEXIO to match the storage mode to trigger the wakeup, but it cannot be achieved

0 Kudos
3 Replies

707 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I was checking if we have some SW example for this mode but it looks like we don't have...

Could you share your configuration which is not working?

Regards,

Lukas

 

0 Kudos

686 Views
584914019
Contributor III

Or provide an example of matching storage mode for me to refer to and operate, see if there is a problem with my understanding

0 Kudos

688 Views
584914019
Contributor III

Yes, I have seen all of your software examples, and I haven’t found any related applications, but your S32K-rm-2019 was first uploaded to chapter 52.4.2.3, which is explained by this matching storage mode. I now want to achieve pause and sleep and re-match So I want to ask you if this function is a function I understand to wake up with the same byte, but this mode cannot be realized.

0 Kudos