S32K SDK RTM vs EAR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K SDK RTM vs EAR

4,629 Views
enricoantonioli
Contributor III

Hi,

I'm starting to develop a new software application for NXP S32K144 and I must choose which SDK can I use.

Which is the diferrence between SDK S32K RTM (release to manufacturing) versus EAR (early access release) quality level in terms of features? Are there any documents that describes these features?

Is there any link where I can get this information?

Best regards,

E.

0 Kudos
Reply
1 Reply

4,040 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

In general, EAR version is not determined for developing application used in production. It is some kind of testing version which should detect bugs and any other potential problems.

If you want to develop new application, I recommend use S32SDK_S32K1xx_RTM_3.0.0, which is the newest RTM version. If you have installed S32 Design Studio with newest update 9, you can see all SDKs in S32DS installation folder.

In these folders, you can find release notes for all versions, please see the figure below:

pastedImage_2.png

Please see the link below to download update 9, which contains latest versions of SDK.

https://community.nxp.com/docs/DOC-342805?sr=search&searchId=8c02f9ef-d654-40e9-9ebc-1af8d30f6aad&se... 

Regards,

Martin

 

0 Kudos
Reply