[S32K] S32DS project name, path and build problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

[S32K] S32DS project name, path and build problem

跳至解决方案
1,787 次查看
carlos_kan
Contributor II

As I have an original project(It may called POT_project), I copy it into a new one, rename it(POT_project_Echoes_Test) and make modification on it. However, when I modify the source files and head files of new project and build the project, I find that the new project still assemble and build files from the old one, as in the configuration of c/c++ build->Settings->Tool Settings->Includes and c/c++ General->Paths and Symbols, these paths all have the file road of the old one.

So if there is a way to change all the old path into new settings, or replace all the old name into a new name?

It seems that I cannot put pic on the message, so I just copy the new project paths to express what I meaning.

In the new POT_project_Echoes_Test,

c/c++ build->Settings->Tool Settings->Includes:

"${workspace_loc:/POT_Project/src/main}" //POT_Project is the original project name

2.png3.png

0 项奖励
回复
1 解答
1,769 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The behavior is correct.

You have to do modification manually or create a new project with desired name and copy headers and source manually.

Best regards,

Peter

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,770 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The behavior is correct.

You have to do modification manually or create a new project with desired name and copy headers and source manually.

Best regards,

Peter

0 项奖励
回复