S32K RTC clock output

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K RTC clock output

1,061 次查看
wanglijun
Contributor II

Hello,

I have a question about the RTC clock output:

In VLPS mode, is there RTC clock output if enabled in RTC module?

 

Thank you!

0 项奖励
回复
1 回复

1,054 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@wanglijun

FF: Full functionality.In VLPR the system frequency is limited,but if a module does not have a function,it is still listed as FF.

Please refer to :S32K RM Table 39-4.Module operation in available power modes(continued)

Senlent_0-1636962880243.png

It shows that RTC was FF in VLPS mode.So I think RTC_CLKOUT should work fine in VLPS.

 

Note: In VLPS mode,FIRC and SPLL clocks should be turned off, so they cannot be selected as RTC reference clocks.

BR!

     Jim,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复