S32K LIN DEMO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K LIN DEMO

1,744 Views
hajianik
Senior Contributor I

Hi,

my target is S32K144. I HAVE TWO BOARDS :

BOARD1 is a PCB representing our production board which has LIN among a whole host of other peripherals.

I've integrated the Master LIN demo in my project .using the scope  I can tell I'm getting some kind of a signal consisting of breaks+sync+id+ data .

I also have a tool that shows the traffic on the bus. there is this message with ID 0X30 and DATA of 0XFD KEEPS SHOWING UP EVERY 5 MS(the rate that the  LIN task runs in my code).

BOARD2 an S32k144 eval board is flashed by the LIN slave mode demo example code.

When I connect the 2 board nothing happens I'll keep getting same packet(ID 0X30 and DATA of 0XFD) as before , no LED turns on/off.

I am not a LIN expert by any means.

The LIN pins are tied together and there's a common ground.

Was wondering do I need to have Master changing some variable on its side to get something changing?

Please help.

Thanks,

Koorosh Hajiani

Tags (1)
0 Kudos
Reply
3 Replies

1,271 Views
Daniel_Wax
NXP Employee
NXP Employee

Are you using the 12 volt power supply on both boards?  You cant use USB 5 volts 

0 Kudos
Reply

1,271 Views
hajianik
Senior Contributor I

Hi Daniel,

That issue has been resolved.

Thanks,

0 Kudos
Reply

249 Views
santhosh23
Contributor III

@hajianik Could you please tell us how did you overcome with this issue?
Even I am facing similar kind of issue.

Thanks & regards,
Santhosh

0 Kudos
Reply