S32K I/O SPEED too slow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K I/O SPEED too slow

1,886 Views
zhengjianfei
Contributor II

HELLO,Recently I discovered  S32K's IO speed is not as fast as i wish。The CPU frq is 112Mhz,bus frq is 56Mhz。The IO speed is 130ns,that is 7.7MHZ。I was not use SDK but directly write the register  PDOR.As usually, IO Speed can reach the half of Bus frq.That is when bus frq is 56MHZ,io speed can reach 26Mhz.But S32K's is just 7.7MHz.Can S32K's io speed faster?

Labels (1)
0 Kudos
Reply
3 Replies

1,631 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Could you please tell me the use case of such an implementation? If you want to generate a PWM signal or toggle GPIO for some timing purposes, you can use hardware peripherals.

There are many variables that influence the frequency. Number of instructions, prefetching, wait states on crossbar switch...

Regards,

Daniel

0 Kudos
Reply

1,631 Views
zhengjianfei
Contributor II

I use GPIO to drive a 16bit LCD。So I need GPIO as fast as it can。

0 Kudos
Reply

1,631 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

I think you can get better results with LMEM Cache:

LMEM->PCCCR = 0x85000001;

Regards,

Daniel

0 Kudos
Reply