S32K GPIO output Voh=? range at 5.0v with 0-5mA current.

cancel
Showing results for 
Search instead for 
Did you mean: 

S32K GPIO output Voh=? range at 5.0v with 0-5mA current.

541 Views
jacky_Tan
NXP Employee
NXP Employee

s32k_GPIO.png

Labels (1)
0 Kudos
3 Replies

414 Views
jacky_Tan
NXP Employee
NXP Employee

thank you Daniel,

would you please provide that customer needs to know the voltage if the pin is loaded with 0mA? no this data in the S32K1xx datasheet.

0 Kudos

414 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jacky,

The output is driven to VDD or VSS.

If the pin is not loaded, the sink/source current is 0mA, the output is equal to VDD or VSS.

Regards,

Daniel

414 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jacky,

What is the question here?

The specification says that the voltage drops to VDD - 0.8V when the pin is loaded with 5 mA.

Regards,

Daniel

0 Kudos