S32K本身不支持FlexRay通讯,但是要是用S32K这个系列的 MCU进行FlexRay接口设计,是否外挂一个FlexRay Communication Controller (例如MRF4300)就可以?
Hi @1396617186
you are right, there's no Flexray module on S32K devices. I'm afraid that MFR4310 is not an option because this device is already in End of Life status.
If Flexray is a must for your application, you can take a look at MPC57xx devices:
Regards,
Lukas
此外,NXP现在还有类似MRF4310这样的Flexray controller 的其他产品吗
Yes, I mean to select different MCU. There are also some other and newer devices with Flexray like S32G, S32E/Z, some S32R but I don't think this is an alternative for S32K. That's the reason why I suggested MPC57xx.
No, NXP does not offer devices similar to MFR4310.
Regards,
Lukas
您好,您的意思更换MCU?