[S32K] Flash memory setting in VLPR Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[S32K] Flash memory setting in VLPR Mode

1,296 Views
jingyinwong
Contributor I

Hi NXP team,

The reference manual of S32K mentions that it is necessary to disable the flash module before turning off FTFC clock prior to entering VLPR mode.

There is no flash driver de-initialize code available in S32 Design Studio. So, what is the right sequence to disable the flash module?

Also, how to verify that FLASH_CLK is already less than or equal to 1MHz?

Thank you.

Best regards,

Jing Yin

Tags (2)
0 Kudos
Reply
1 Reply

1,163 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,
There is no need to disable the FTFC module before entering VLPR. The VLPR clock configuration must be done before the transition.
In VLPR, no FTFC commands of any type are available and the Flash clock is restricted to 1MHz or less.
The Flash clock can be monitored externally at a CLKOUT pin. Please see Figure 27-1 RM rev.9

pastedImage_1.png

Regards,
Daniel

0 Kudos
Reply