S32K EB tresos SPI configuration DMA and slave mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K EB tresos SPI configuration DMA and slave mode

2,552 Views
Simin
Contributor II

hi,

    According to Autosar MCAL SPI driver SRS、SWS document,there is not any requirement or

definition about SPI using DMA function and SPI woking in slave mode,but we can enable SPI

DMA function and configuration SPI in slave mode via S32K14X EB tresos tool,Does this use conform to

AUTOSAR standards and why?

Best regards,

Jack

Tags (4)
0 Kudos
Reply
4 Replies

2,522 Views
namnguyenviet
NXP Employee
NXP Employee

As per my understanding, yes, if your application doesn't require to strictly compliant with AUTOSAR for all of the features. 

0 Kudos
Reply

2,519 Views
Simin
Contributor II

Hi Nam,

    Got it,thanks for your kind feedback

Best regards,

Jack

 

0 Kudos
Reply

2,536 Views
namnguyenviet
NXP Employee
NXP Employee

Hello,

SPI slave support feature and SPI DMA feature are both non-AUTOSAR.

Best Regards,

Nam

0 Kudos
Reply

2,530 Views
Simin
Contributor II

Hi Nam,

    Does such a non-AUTOSAR feature can be used in the environment of AUTOSAR?

Best regards,

Jack

0 Kudos
Reply