S32K ADC PAL Conversion groups configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K ADC PAL Conversion groups configuration

1,579件の閲覧回数
thulzh
Contributor III

Hi,

    The project that I am working in needs to convert 15 channels using ADC0 and 3 channels using ADC1.

     When I use RTM4.0.2 to configure the ADC modules with ADC_PAL_Configuration, I fails to get the correct converting result if I set one ADC0 conversion group where there are 15 adc0 channels and set one ADC1 conversion group where there are 3 adc1 channels.  The results which should appear in the adc_pal_0_result0[]  appear in adc_pal_1_result0[]. When I set two ADC0 conversion groups, contain 8 and 7 channels seperately, the conversion results are in line with expectations.

      What is the difference between these two configuration?

 

0 件の賞賛
返信
1 返信

1,553件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @thulzh,

Can you please share the whole project so that I can test it?

 

Thank you,

BR, Daniel

0 件の賞賛
返信