S32K ADC CONFIG

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K ADC CONFIG

1,272 Views
liulei1
Contributor II

I configured the ADC program, the voltage value and the result of the routine in S32DS are different by 0.9V. Why is this? Is it because I am using software triggering, is the routine using hardware triggering?

ADC_MemMapPtr ADCx[2] = {ADC0, ADC1}; //定义两个指针数组保存 ADCx 的地址
void adc_DMA_init(TYP_ADCn adcn, TYP_ADC_Ch ch)
{

adc_init(adcn, ch) ;//初始化ADC时钟
adc_stop(adcn);

ADCx[adcn]->SC2 = ADTRG_HW //硬件触发
| ACFE_DISABLED
|ACFGT_LESS//| ACFGT_GREATER
| ACREN_DISABLED
| DMAEN_DISABLED
| ADC_SC2_REFSEL(REFSEL_EXT);

ADCx[adcn]->SC3 = CAL_OFF
|ADCO_SINGLE//| ADCO_CONTINUOUS
| AVGE_DISABLED
| ADC_SC3_AVGS(AVGS_4);
ADCx[adcn]->SC1[0] = AIEN_OFF | DIFF_SINGLE |
ADC_SC1_ADCH( ch );
}
void adc_init(TYP_ADCn adcn, TYP_ADC_Ch ch)
{

switch(adcn)
{
case SADC0: /* ADC0 */
PCC->PCCn[PCC_ADC0_INDEX] &=~ PCC_PCCn_CGC_MASK;
PCC->PCCn[PCC_ADC0_INDEX] = PCC_PCCn_CGC_MASK | PCC_PCCn_PCS(1); 

switch(ch)
{
case AD0: //ADC0_SE0-- PTA0
PORTA->PCR[0] |= PORT_PCR_MUX(0);
break;
case AD1: //ADC0_SE1-- PTA1
PORTA->PCR[1] |= PORT_PCR_MUX(0);
break;
case AD2: //ADC0_SE2-- PTA6
PORTA->PCR[6] |= PORT_PCR_MUX(0);
break;
case AD3: //ADC0_SE3-- PTA7
PORTA->PCR[7] |= PORT_PCR_MUX(0);
break;
case AD4: //ADC0_SE4-- PTB0
PORTB->PCR[0] |= PORT_PCR_MUX(0);
break;
case AD5: //ADC0_SE5 -- PTB1
PORTB->PCR[1] |= PORT_PCR_MUX(0);
break;
case AD6: //ADC0_SE6 -- PTB2
PORTB->PCR[2] |= PORT_PCR_MUX(0);
break;
case AD7: //ADC0_SE7 -- PTB3
PORTB->PCR[3] |= PORT_PCR_MUX(0);
break;
case AD8: //ADC0_SE8 -- PTC0
PORTC->PCR[0] |= PORT_PCR_MUX(0);
break;
case AD9: //ADC0_SE9 -- PTC1
PORTC->PCR[1] |= PORT_PCR_MUX(0);
break;
case AD10: //ADC0_SE10 -- PTC2
PORTC->PCR[2] |= PORT_PCR_MUX(0);
break;
case AD11: //ADC0_SE11 -- PTC3
PORTC->PCR[3] |= PORT_PCR_MUX(0);
break;
case AD12: //ADC0_SE12 -- PTC14
PORTC->PCR[14] |= PORT_PCR_MUX(0);
break;
case AD13: //ADC0_SE13 -- PTC15
PORTC->PCR[15] |= PORT_PCR_MUX(0);
break;
case AD14: //ADC0_SE14 -- PTC16
PORTC->PCR[16] |= PORT_PCR_MUX(0);
break;
case AD15: //ADC0_SE15 -- PTC17
PORTC->PCR[17] |= PORT_PCR_MUX(0);
break;

default:
break;
}
break;

case SADC1: /* ADC1 */
PCC->PCCn[PCC_ADC1_INDEX] &=~ PCC_PCCn_CGC_MASK;
PCC->PCCn[PCC_ADC1_INDEX] = PCC_PCCn_CGC_MASK | PCC_PCCn_PCS(1); 
switch(ch)
{
case AD0: //ADC1_SE0-- PTA2
PORTA->PCR[2] |= PORT_PCR_MUX(0);
break;
case AD1: //ADC1_SE1-- PTA3
PORTA->PCR[3] |= PORT_PCR_MUX(0);
break;
case AD2: //ADC1_SE2-- PTD2
PORTD->PCR[2] |= PORT_PCR_MUX(0);
break;
case AD3: //ADC1_SE3-- PTD3
PORTD->PCR[3] |= PORT_PCR_MUX(0);
break;
case AD4: //ADC1_SE4 -- PTC6
PORTC->PCR[6] |= PORT_PCR_MUX(0);
break;
case AD5: //ADC1_SE5 -- PTC7
PORTC->PCR[7] |= PORT_PCR_MUX(0);
break;
case AD6: //ADC1_SE6 -- PTD4
PORTD->PCR[4] |= PORT_PCR_MUX(0);
break;
case AD7: //ADC1_SE7 -- PTB12
PORTB->PCR[12] |= PORT_PCR_MUX(0);
break;
case AD8: //ADC1_SE8 -- PTB13
PORTB->PCR[13] |= PORT_PCR_MUX(0);
break;
case AD9: //ADC1_SE9 -- PTB14
PORTB->PCR[14] |= PORT_PCR_MUX(0);
break;
case AD10: //ADC1_SE10 -- PTE2
PORTE->PCR[2] |= PORT_PCR_MUX(0);
break;
case AD11: //ADC1_SE11 -- PTE6
PORTE->PCR[6] |= PORT_PCR_MUX(0);
break;
case AD12: //ADC1_SE12 -- PTA15
PORTA->PCR[15] |= PORT_PCR_MUX(0);
break;
case AD13: //ADC1_SE13 -- PTA16
PORTA->PCR[16] |= PORT_PCR_MUX(0);
break;
case AD14: //ADC1_SE14 -- PTB15
PORTB->PCR[15] |= PORT_PCR_MUX(0);
break;
case AD15: //ADC1_SE15 -- PTB16
PORTB->PCR[16] |= PORT_PCR_MUX(0);
break;

default:
break;
}
break;
default:
break;
}
}
uint16_t ad_once(TYP_ADCn adcn, TYP_ADC_Ch ch, TYP_ADC_nbit bit)
{
uint16_t result = 0;


adc_start(adcn, ch, bit); //启动ADC转换
while (( ADCx[adcn]->SC1[0] & ADC_SC1_COCO_MASK ) != ADC_SC1_COCO_MASK);
result = ADCx[adcn]->R[0];
ADCx[adcn]->SC1[0] &= ~ADC_SC1_COCO_MASK;
return result;
}
uint16_t ad_ave(TYP_ADCn adcn, TYP_ADC_Ch ch, TYP_ADC_nbit bit, uint8_t N)
{
uint32_t tmp = 0;
uint8_t i;

for(i = 0; i < N; i++)
tmp += ad_once(adcn, ch, bit);
tmp = tmp / N;
return (uint16_t)tmp;
}
void adc_start(TYP_ADCn adcn, TYP_ADC_Ch ch, TYP_ADC_nbit bit)
{

//ADCx[adcn]->CFG1 = 0x000000004;
/* ADICLK=0: Input clk=ALTCLK1=SOSCDIV2 */
/* ADIV=0: Prescaler=1 */
/* MODE=1: 12-bit conversion */
ADCx[adcn]->CFG1 = ADLPC_NORMAL
| ADC_CFG1_ADIV(ADIV_1)//| ADC_CFG1_ADIV(ADIV_4)
| ADC_CFG1_MODE(bit)
| ADC_CFG1_ADICLK(ADICLK_BUS);
ADCx[adcn]->CFG2 = ADC_CFG2_SMPLTS(150);
// ADC_SC2_REG (ADCx[adcn]) =
// | ADACKEN_DISABLED
// | ADHSC_HISPEED
// | ADC_CFG2_ADLSTS(ADLSTS_20) ;
ADCx[adcn]->SC1[0] = DIFF_SINGLE | ADC_SC1_ADCH( ch );
}

Register result as so:

pastedImage_1.png

pastedImage_2.png

0 Kudos
Reply
1 Reply

1,017 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Have you calibrated the ADC module?

It doesn't matter whether you use HW or SW triggers.

But it depends on the signal that you are measuring, the sampling rate, Rs, Cf...

Please measure the signal with an oscilloscope.

Regards,

Daniel 

0 Kudos
Reply