Hello, I am configuring the port part of MCAL in S32K144, but once I enable this function, the chip will lock after writing, and cannot connect to the debugger any more, so it needs to be unlocked again.When I don't use the portinit function, the software works fine, Could you please help me to see if there is any problem with my relevant configuration
Hi
Note that these debug pins should be added to UnTouchedPortPin.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------