下载了IDE 和 CodeWarrior 不知道有没有官方维护的库函数,因为之前使用STM32的库函数和CUBEMX的可视化配置,不知道S32K 和 MC9S12G 有没有?
Hi
I have installed:
But in S32 Configuration Tool
but this is missing
No SDK are found
is the same here with sdk
For S32K:
Yes. Please download S32 Design Studio 3.4 – Windows/Linux(REV 3.4) and install S32SDK S32K1XX RTM 4.0.1 then use S32 Configuration Tool.
You can read the S32_Configuration_Tools_Release_Notes for more detail about how to use it(C:\NXP\S32DS.3.4\Release_Notes)
For MC9S12G, please ask question in S12 / MagniV Microcontrollers.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------