S32DS / S32K142: holding low the UART tx pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS / S32K142: holding low the UART tx pin

1,078 Views
kwakd_y
Contributor III


I'm using UART to interface with a chip which implements a "safe mode" UART configuration in which the chip runs it's UART port with a standard, known parameters set - this allow recovering from configuration errors.

 

To trigger such "safe mode" I need to hold UART Tx at low, for a predefined, long time. What would be the best way to accomplish that? Changing the port configuration to GPIO, and than back to UART?

I try to firat set UART Configration and then second set GPIO. But not conversion to GPIO.

Help me Plase.

<1>

void Uart_SetUArt0(void)  /* Init. summary: 500000 baud, 1 stop bit, 8 bit format, no parity */
{
  PCC->PCCn[PCC_LPUART0_INDEX] &= ~PCC_PCCn_CGC_MASK;    /* Ensure clk disabled for config */
  PCC->PCCn[PCC_LPUART0_INDEX] |= PCC_PCCn_PCS(6)    /* Clock Src= 1 (SOSCDIV2_CLK) */
                               |  PCC_PCCn_CGC_MASK;     /* Enable clock for LPUART1 regs */

  LPUART0->BAUD =0x09000002;    /* SBR = 2, OSR = 10(9+1), 10,000,000/(2*10) = 500,000 */

  LPUART0->CTRL=0x002C0000;    /* Enable transmitter & receiver, no parity, 8 bit char: */
                               /* RE=1: Receiver enabled */
                               /* TE=1: Transmitter enabled */
                               /* PE,PT=0: No hw parity generation or checking */
                               /* M7,M,R8T9,R9T8=0: 8-bit data characters*/
                               /* DOZEEN=0: LPUART enabled in Doze mode */
                               /* ORIE,NEIE,FEIE,PEIE,TIE,TCIE,RIE,ILIE,MA1IE,MA2IE=0: no IRQ*/
                               /* TxDIR=0: TxD pin is input if in single-wire mode */
                               /* TXINV=0: TRansmit data not inverted */
                               /* RWU,WAKE=0: normal operation; rcvr not in statndby */
                               /* IDLCFG=0: one idle character */
                               /* ILT=0: Idle char bit count starts after start bit */
                               /* SBK=0: Normal transmitter operation - no break char */
                               /* LOOPS,RSRC=0: no loop back */

}

 PCC->PCCn[PCC_PORTC_INDEX ]|=PCC_PCCn_CGC_MASK;  /* Enable clock for PORTC */
 PORTC->PCR[2]|=PORT_PCR_MUX(4);              /* Port C2: MUX = ALT4,UART0 RX */
 PORTC->PCR[3]|=PORT_PCR_MUX(4);              /* Port C3: MUX = ALT4,UART0 TX */

<2>

 PCC->PCCn[PCC_PORTC_INDEX ]|= PCC_PCCn_CGC_MASK;  /* Enable clock for PORT */
 PORTC->PCR[3]|=PORT_PCR_MUX(1);              /* GPIO OUT */
 PTC->PDDR |= 1<<3;
 PTC->PCOR |= 1<<3;         /* LOW */ 

Best regards,

kwak

0 Kudos
1 Reply

952 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello kwakd.y,

You solution should work.

If I understand, you are not able to reconfigure the port to GPIO.

I guess this is because you read-modify-write the PCR register. 

Your code:

PORTC->PCR[3]|=PORT_PCR_MUX(4); 

PORTC->PCR[3]|=PORT_PCR_MUX(1);

sets the PCR_MUX to 0x5 = 0x4 | 0x1.

How long does the TX pin need to be low?

The LPUART can send a break character:

pastedImage_1.png

BR, Daniel

0 Kudos