S32DS 3.6 issue with get the RTD working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS 3.6 issue with get the RTD working

Jump to solution
683 Views
Bridgebranch
Contributor II

Hi NXP team,

I'm working with S32K144 using

S32 Design Studio v3.6 and S32K1_S32M24X Real Time Drivers AUTOSAR R21-11 Version 3.0.0

I followed this tutorial to set up a simple LED blink using the RTD drivers:
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-example-pr...

However, when adding the Port_Ip component in the .mex file, I get this error:

Bridgebranch_0-1746814786275.png

And if i delet and add the Port_Ip_1 i get it to work but when I try to build the project I get this error.

Bridgebranch_1-1746815299829.png

Thx for the support

 

 

0 Kudos
Reply
1 Solution
658 Views
Bridgebranch
Contributor II

It was just a simple mistake wrong name in the guide. it is now fixed.

 

/M

View solution in original post

0 Kudos
Reply
2 Replies
659 Views
Bridgebranch
Contributor II

It was just a simple mistake wrong name in the guide. it is now fixed.

 

/M

0 Kudos
Reply
663 Views
Bridgebranch
Contributor II
Hi, so now I update to 3.6.1 and got the IP issue solved. now only the issue wtih 'g_pin_mux_InitConfigArr0' undeclared (first use in this function). Not working.


0 Kudos
Reply