S32DS 2018.R1 doesn't recognize OpenSDA COM port on S32K144 EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS 2018.R1 doesn't recognize OpenSDA COM port on S32K144 EVB

Jump to solution
1,526 Views
davorin_mista
Contributor I

I'm trying to debug an application on my S32K144EVB using S32DS 2018.R1 Update11, running the example project BCC_S32K144_Monitoring: 

Hardware: S32K144EVB-Q100 + FRDM33771CSPEVB = BATT-14EMU
The EVB is powered on, running the pre-built BMS example from the Freedom Board "MC3377xC EvalGUI"

Device Manager shows COM7 as OpenSDA, yet S32DS Debug Configurations doesn't give me a debug port to choose.I freshly rebooted Windows to make sure I don't have any other application running that may be hogging the COM7 port.

Also using TeraTerm I can connect to COM7, further indicating that the port is not in use already.

davorin_mista_0-1672258404719.png

Please advise.

Thanks,
Davorin

0 Kudos
Reply
1 Solution
1,507 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is possible. Current PeMicro OpenSDA Debug Driver is dated January 23rd, 2017 so it is newer than yours. You may download it here:

https://www.pemicro.com/opensda/index.cfm

 

View solution in original post

0 Kudos
Reply
3 Replies
1,498 Views
davorin_mista
Contributor I

Fwiw, uninstalling both my S32DS versions as well as the PEMicro drivers - and then only installing 2018.R1 fixed my issue. Maybe I could have also just uninstalled the drivers and installed the one you suggested...

0 Kudos
Reply
1,518 Views
davorin_mista
Contributor I

I just noticed these 3 drivers in Device Manager:

davorin_mista_0-1672270163801.png

Could this be the cause of my issues? 

"PEMicro ..." driver is version 12.3 from 2/18/2016

"pemicrowindrvr" is version 12.4 from 1/4/2017

WinDriver is also version 12.3 from 2/18/2016

Which one(s), if any, shall I remove?

Thanks,
Davorin

0 Kudos
Reply
1,508 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is possible. Current PeMicro OpenSDA Debug Driver is dated January 23rd, 2017 so it is newer than yours. You may download it here:

https://www.pemicro.com/opensda/index.cfm

 

0 Kudos
Reply