S32144-LOC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
600件の閲覧回数
Junkie
Contributor I

May I ask if the S32K144 software does not operate properly and triggers SOSCERR to be set when the SOSC clock monitor is turned on? I tried entering (all) low power modes after turning on the clock monitor, and I can see that SOSC becomes invalid (SOSCVLD=0) but no SOSCERR is generated.

0 件の賞賛
1 解決策
558件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Well, I can't see simple way how to inject this error by software. As you mentioned, for test purposes such error is usually injected by shorting of OSC circuit in hardware.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
4 返答(返信)
568件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm not sure if I can understand the question but clock monitors should not be used in low power modes:

lukaszadrapa_0-1660033659856.png

Regards,

Lukas

0 件の賞賛
563件の閲覧回数
Junkie
Contributor I

Yes, it is mentioned in the reference manual that SOSC monitor cannot be used in low power mode. But my purpose is to cause a LOC error to reset the MCU, I caused the LOC error by shorting the external SOSC crystal to ground, but is there a way to use software? I've tried going into low power mode to cause the LOC error but it doesn't work.

0 件の賞賛
559件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Well, I can't see simple way how to inject this error by software. As you mentioned, for test purposes such error is usually injected by shorting of OSC circuit in hardware.

Regards,

Lukas

0 件の賞賛
493件の閲覧回数
Junkie
Contributor I
OK, thank you very much.
0 件の賞賛