doz not help.. can you provide example how to read potentiometer R84 voltage on the MR-CANHUBK344 board?
how to configure group of external ADC to read?
Hi @paulffffff,
Please refer to the example from the RTD package (Adc_Sar_Bctu_Ip_example_S32K344
Which uses the software trigger to trigger ADC normal and injected conversions, also software trigger from BCTU. You can just modify the channel to ADC1_S10 or whichever channel you need in the configuration.
Best regards,
Julián
Hi @paulffffff,
You can change the channel from the AdcConfigSet and under AdcHwUnit:
Best regards,
Julián
can you provide example how to read voltage (R84 resistor) on MR-CANHUBk344 board?
Also, any other ADC pin to configure for readings?
Hi @paulffffff,
Please take a look into the following community post for guidance on MR-CANHUBK344 projects and how to use de inputs/outputs: Interacting with Digital Inputs/Outputs on MR-CANHUBK344 - NXP Community
Also, you can find which pin, adc channel and resistor is connected in the board in chapter 6.13 from the MR-CANHUBK344 Hardware User Manual
Best regards,
Julián