S32 Design studio project no "ARM EWL" libraries support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design studio project no "ARM EWL" libraries support

566件の閲覧回数
LeoZ
Contributor III

when I refer Example S32K_printf_implementation - S32DS_1.0 - NXP Community this topic,

it mentioned bellow 'libraries support' setting, 

ref_old.jpg

 

but in my project, there is no this selection,

my environment: S32 Design Studio 3.5, MCU: S32K358

rer_new.jpg

how could I add aforementioned "ewl_c" selection 

0 件の賞賛
4 返答(返信)

552件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi LeoZ,

Do you want to implement printf by LPUART peripheral, or by Semihosting when debugging?  Attached project implementing Printf by UART, it is based on S32DS v3.4 + S32K3 RTD 0.9.0. Although the RTD version and part number are different, I hope it will be helpful to you.

Best Regards,
Robin

0 件の賞賛

526件の閲覧回数
LeoZ
Contributor III

Thank you, I want to use printf for uart, and I succeeded in S32K358 referring to your project. 

While I found it can not send floating number, then I refer to 浮点数在串口打印的函数  to convert float number to string to send,

I do not know if there is better way to print floating number

printf_data.jpg

0 件の賞賛

498件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Did you checked the Support printf float format for newlib_nano library (-u_printf_float) ?

Support printf float format for newlib_nano library.png

0 件の賞賛

490件の閲覧回数
LeoZ
Contributor III

thank you, checking that solved my problem

btw: from the warning, it takes '(float32) a' as a double,  I am not sure if it will cost more uart time to take 'a' as double than single-floating, (if so) then if existing some way to modify printf for it. anyway, this question is not important, just curious.

xxxxxxxxx7.jpg

0 件の賞賛