For the S32K144 Development Board。
I download one project by S32 Design stdudio ,some error showed when build the project。
Even if I add header files to the project, I still report an error
Solved! Go to Solution.
change highlighted jumper to 2 & 3 and try again.
All of your problems come from not reading the guide to becoming familiar with your development environment.
I can't help you without more info.
Can you provide more info about your problem, such as the version of IDE and SDK,also the project you downloaded and the build error log.
HI Senlent
the version:S32 Design Studio for ARM Version 2.2
T he ifo of error;
Thank you.
I see that you have added the paths of these files.
Maybe you should first check whether these files are under your project folder.
HI Senlent
I initially thought the header file was missing, but it actually exists
AS the following figure
After this problem appeared, I found some solutions online. For example, adding header files has no effect
So need your help for give some recommendations to closed the error。
Thanks
I'd like to help you,Is it possible to provide a project so that I can reproduce the problem?
I just imported the compressed package you provided, and there was no problem with compilation.
HI Senlent
Using the following import,which I need to choose in the item?
I used to use Open projects from file system
HI Senlent
This project Compilation passed,but i can't find the download options 0.0
HI Senlent
After build the project,This window pops up,I try some way to change the config,but never resolved
Is this your first using S32 DS?
Can other projects be connected normally?
Can you refer to the debugging interface configuration of a normally working project?
HI Senlent
yes,It’s the frist time to use S32 DS,when I download the APP,the problem is bothering me until now。
So in use the APP,so much questions perplex me。Luckly, this forum exists
good news, if your problem are solved, you can click "ACCEPT AS SOLUTION" to close this topic.
HI Senlent
This is the development board I am using. What should be its interface configuration to solve this problem
change highlighted jumper to 2 & 3 and try again.
All of your problems come from not reading the guide to becoming familiar with your development environment.