I am trying to use DS32 Design Studio for configure the pins of S32K8xx. DS32 does not work with the K3 family. When I create the project there is no MCU selected. In the image showing the steps there does not seem to be an SDK available for selection. Is there a way to resolve this?
I added the package like you described above. The S32K388 is now available which is good. However, I still cant do the pin configuration as there is no SDK in the drop down list when I create the project.