S32 Design Studio not working with S32K3xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio not working with S32K3xx

5,628 Views
mark2468
Contributor II

Hi.

I am trying to use DS32 Design Studio for configure the pins of S32K8xx. DS32 does not work with the K3 family. When I create the project there is no MCU selected. In the image showing the steps there does not seem to be an SDK available for selection. Is there a way to resolve this?

Thanks.

Tags (2)
0 Kudos
Reply
8 Replies

5,583 Views
mark2468
Contributor II

I didn't try the RTD as I had reinstalled version V3.4 and everything worked.

 

As it turns out V3.4 does not support all the S32K3xx devices so I might have to try V3.5 again to use these devices.

0 Kudos
Reply

5,614 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @mark2468,

You need to install the S32 Design Studio 3.5.0 development packages for offline use, support for S32K3xx, S32K358 and S32K388 package

danielmartynek_0-1677770437926.png

https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32k-auto-gener...

 

Automotive SW - S32K3 - S32 Design Studio

3.5.0_D2212 S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices 

Download SW32K3xx.S32DS_3.5.0_D2212.zip

Add it as an Update site

danielmartynek_1-1677770627200.png

After that, you should see it in the Available/Update list

 

BR, Daniel

 

 

 

5,569 Views
mark2468
Contributor II

I added the package like you described above. The S32K388 is now available which is good. However, I still cant do the pin configuration as there is no SDK in the drop down list when I create the project.

 

Do I need to add something else for this?

 

Thanks.

0 Kudos
Reply

5,612 Views
mark2468
Contributor II

It is available in the update list but it wont install. I get the error shown in the image.

 

Any suggestions?

0 Kudos
Reply

5,604 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @mark2468,

The library requires RTD 2.0.1.

It might be in the list already, if not, you can find it again in the Standard Software

Automotive SW - S32K3 - Real-Time Drivers for Cortex-M

S32K3 Real-Time Drivers Version 2.0.1

 

Regards,

Daniel

5,598 Views
mark2468
Contributor II

Thanks for the reply.

 

I downgraded to V3.4 and everything works. I think there is an issue with V3.5

 

Mark.

4,998 Views
Anjalipurushothaman
Contributor III

will the S32ds studio version 3.4 support family S32K388 OR S32K358?

0 Kudos
Reply

5,586 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Do you mean you can't install the RTD 2.0.1 or the library in S32DS 3.5?

 

Thanks,

Daniel

0 Kudos
Reply