S32 Design Studio V3.5 with S32K311

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio V3.5 with S32K311

2,180 Views
vanketnguyen
NXP Employee
NXP Employee

I use S32K311.

I am using S32DS V3.5  with installed S32K3xx Development Package Version 3.5. RTM + S32K3 RTD AUTOSAR R21-11 Version 3.0.0 (please attachment)

 

1. I could not create a new project when selecting K311.

2. I tried to import any example of K311 but there is no example for K311 or even K31x.

Could you help to advise?

 

Van Ket

0 Kudos
2 Replies

2,107 Views
NamLee
NXP Employee
NXP Employee

Dear vanketnguyen,

Sorry for lately reply, the NXP site was down last week and i just checked your ticket in this week.

Firstly, the DS example only support for derivatives that you mentioned, so unfortunately, it's not available for K311 as you said.

I think you can try to create your own project.

NamLe_0-1690277564140.png

Secondly, i saw an option in SDK selection for K311 as below, when i try to create a new project for K311.

NamLe_1-1690277985747.png

 

I think there're some points that you can check again:

- Firstly, you can try to uninstall the S32K3 RTD Version 3.0.0 then Install the S32K3XX RTD Version 3.0.0 (which is the version that i installed)

- In case that doesn't work, please follow this instruction:

    + Uninstall the DS and clear folder/files if any left.

    + Install the DS 3.5 again (i'm using S32DS.3.5_b220726_win32.x86_64 exe file)

    + Install K3 development package (and related requirements also)

    + Install the S32K3XX RTD Version 3.0.0 (which is the version that i installed)

Be aware that you need to accept all requirements during installation.

Please let me know if you have any further information.

Thank you,

Nam.

0 Kudos

2,178 Views
vanketnguyen
NXP Employee
NXP Employee

Here are the attachments.

0 Kudos