S32 Configuration tool - SPI configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Configuration tool - SPI configuration

ソリューションへジャンプ
5,315件の閲覧回数
SivakumarMariappan
Contributor II

Hello 

I'm using the S32 Configuration tool to configure the SPI peripheral as a master in MCU. We are getting 2 options , when I choose the LPSPI0 peripheral. Please refer the "SPI_Peripheral_Options" screenshot. Also I have attached the screenshot for for both options. We would like to use it in a polling method and transfer 512 bytes of data at every 10mSec loop. Also we could see only 2 options in transfer types. 1. DMA 2. Interrupt. Do we need to choose DMA for polling method please? Do we need to choose the SPI Driver option or SPI PAL please? what is the difference between these 2 options please?

0 件の賞賛
返信
1 解決策
5,290件の閲覧回数
SivakumarMariappan
Contributor II

Many thanks Senlent.

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,291件の閲覧回数
SivakumarMariappan
Contributor II

Many thanks Senlent.

 

0 件の賞賛
返信
5,296件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@SivakumarMariappan

1.No,interrupt method will be ok.

2.In this picture you can see the difference between PAL and PD.

Senlent_0-1680573112536.png

 

0 件の賞賛
返信