S32 Configuration tool - SPI configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 Configuration tool - SPI configuration

跳至解决方案
5,362 次查看
SivakumarMariappan
Contributor II

Hello 

I'm using the S32 Configuration tool to configure the SPI peripheral as a master in MCU. We are getting 2 options , when I choose the LPSPI0 peripheral. Please refer the "SPI_Peripheral_Options" screenshot. Also I have attached the screenshot for for both options. We would like to use it in a polling method and transfer 512 bytes of data at every 10mSec loop. Also we could see only 2 options in transfer types. 1. DMA 2. Interrupt. Do we need to choose DMA for polling method please? Do we need to choose the SPI Driver option or SPI PAL please? what is the difference between these 2 options please?

0 项奖励
回复
1 解答
5,337 次查看
SivakumarMariappan
Contributor II

Many thanks Senlent.

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
5,338 次查看
SivakumarMariappan
Contributor II

Many thanks Senlent.

 

0 项奖励
回复
5,343 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@SivakumarMariappan

1.No,interrupt method will be ok.

2.In this picture you can see the difference between PAL and PD.

Senlent_0-1680573112536.png

 

0 项奖励
回复