Reserve ADC S32K148

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reserve ADC S32K148

2,979 Views
hamid_abrishami
Contributor III

Hi every one.
I want to use FS32K148HAT0MLUT micro controller in my project. I reed reference manual and i found out that some of the  ADC is reserved and one of them is used as power supply monitoring.
after that I search in S32K148_IO_Signal_description_Input_Multyplexing about reserve ADC but I didn't see any thing about that . 
Can I use them in my project as analog input or no? (picture of 43-3 is attached from reference manual) 
 
thanks

Tags (1)
0 Kudos
Reply
3 Replies

2,943 Views
hamid_abrishami
Contributor III

I find out that we can use ADC0_ch0 as in put and all other internal reserved ADC according to some EVAL board that use them as ADC in put. 

0 Kudos
Reply

2,964 Views
Senlent
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,945 Views
hamid_abrishami
Contributor III

Hi
I don't want to use internal ADC. I just want to be sure that I Can use all the ADC pins as input 

0 Kudos
Reply