I am everett a fae of nxp,I need request access to the SafeAssure NDA group to support our customers
I'm FUSA engineer of Valeo Interior Controls (Shenzhen) Co.,Ltd.
There's ASILD project using two ASILB MCU, one of two is MC2: FS32K116BRT0VLFR which is used for slave function.
for MC2, no CAN transmission, just have the communication with MC1, MC1 send out the CAN message.
so there're some SMs and functions not implemented, need NXP help to re-calculate the MC2 FMEDA.
1. SM_075&SM_076 are not implemented. no CAN message leads to remove external clocks replaced by MC2 internal clock. MC2 internal clock accuracy ensured by MC1 synchronize;
2. SM_114 is not implemented, because no FUSA data is stored in EEPROM;
3, no eDMA transmission, just use CPU transmission.
Please help to re-calculate the MC2 FMEDA.
thanks~
Hi@RandyZM
Sorry for not being able to answer your question.
You can ask questions about functional safety in this forum
or get support from these channel.
submit a ticket from the link below.
https://www.nxp.com/support/support:SUPPORTHOME
please refer to following links.
BR!
Jim,
thanks,solved