Regarding BMS SDK for S32K344

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding BMS SDK for S32K344

1,139 Views
tetsuya_nakamur
Contributor III

 

The customer is having trouble incorporating the BMS SDK into the IDE environment.

I have attached the contents, so please check it.

Please let me know the cause and solution.

I'm sorry, but please answer by 8/23.

 

0 Kudos
Reply
3 Replies

1,097 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello tetsuya_nakamur,

I hope all is great with you. Thank you for using the NXP communities.

As mentioned on the case created, I do recommend using the HVBMS Software Installation Guide as a reference.

Please go to Software section and click on Automotive Software Package manager from the link below:

https://www.nxp.com/design/designs/hvbms-reference-design-bundle-using-etpl:RD-HVBMSCTBUN

I hope this information helps.

Regards,

David

0 Kudos
Reply

1,044 Views
tetsuya_nakamur
Contributor III

 

Dear David-san,

 

It does not solve the problem yet.

 

But, the customer downloaded the material you answered and followed the steps in "5.1.2.3 BMS Software Development Kit", but SW32K3_BMS_SDK_4.4_0.9.0_D2210.exe was already installed.

 

tetsuya_nakamur_0-1693294914993.png

 

 

Also, I found 1.0.0 (D2304), which is newer than version 0.9.0 (D2210),I uninstalled 0.9.0 and installed 1.0.0,

the result was the same (Create a new project: BMS SDK is not displayed in the SDK selection column).

 

[Question]

1.After all, which of the following is the correct way to install the BMU SDK?

 a) Installer (SW32K3_BMS_SDK_4.4_1.0.0_D2304.exe)

 b) S32DS Help-Install new software menu (SW32K3_BMS_SDK_4.4_1.0.0_updatesite_2304.zip)

 

tetsuya_nakamur_1-1693294915021.png

 

 

tetsuya_nakamur_2-1693294915044.png

 

 

2.Also, please answer any other solution.

 

Best Regards,

AVNET

Tetsuya Nakamura

 

0 Kudos
Reply

1,032 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello tetsuya_nakamur

In response to my request for further information, our specialist has concluded that we need the following information to better understand the situation.

  1. Are you using a HVBMS bundle board?
  2. What example are you trying to run?
  3. Have you run the HvBms400_775_772_TPL_Bring_Up  example?

You may review the last reply at the case created for further information. 

Regards,

David 

0 Kudos
Reply