RappID Tool for S32K144

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RappID Tool for S32K144

2,619件の閲覧回数
gopichakrala
Contributor I

Hi Nxp Team,

I have gone through the user manual of RAPPID tool and fallowed the below steps

1. Drag and drop the RBF file o the Evaluvation board

2.reset the EVAL board(connected the S32K144 Eval board with USB)

3. open the Rappid tool

4.load the rbl file (given in the example project of S32K_bootloader ,edited the path in the rbl file)

5. tool updated the all the configuration details and click on the "start the bootloader"

but it is not programmed , it is showing error "loss communication with CCP MCU, please cycle power and try again" and "operation has timed out".

I have tried with reset the controller and tried , but still getting same error.

for the application download also, manually i have set the configuration details and and disable the "BAM status" , tried to flash the Timer_test.hex file ,still it is showing same error.

find the attached errors images and please let me know the solution.

Regards,

Gopi

ラベル(1)
0 件の賞賛
返信
1 返信

2,017件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

please check this thread:

https://community.nxp.com/thread/469590 

Stan

0 件の賞賛
返信