RTD version update question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RTD version update question

1,208 次查看
focusdoit
Contributor III

Hi Nxp experts,

I have a project created on RTD SW32K3_S32M27x_RTD_R21-11_4.0.0 on EB tresos, now I want to switch to RTD SW32K3_S32M27x_RTD_R21-11_4.0.0_P19.

Can I just replace the old link file SW32K3_S32M27x_RTD_R21-11_4.0.0.link with the new link file SW32K3_S32M27x_RTD_R21-11_4.0.0_P19.link?

Thanks

0 项奖励
回复
3 回复数

1,183 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @focusdoit 

During the installation of the .exe, you can select the EB Tresos installation directory or you can copy all "<mod>_TS_T40D34M40I0R0" directories and .JAR files to the "<Tresos Install Path>\plugins" directory.

 

B.R.

VaneB

0 项奖励
回复

1,180 次查看
focusdoit
Contributor III

I mean the modules configured on old RTD, such as, Adc.xdm, Dem.xdm, Dio.xdm, Spi.xdum .. etc, can switch these configurations  to the new RTD smoothly?

0 项奖励
回复

1,145 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @focusdoit 

The project maintains the files from the previous version. I am afraid that it will be required to create a new project with the new RTD version. 

0 项奖励
回复