RTD naming question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTD naming question

934件の閲覧回数
focusdoit
Contributor III

Hi NXP experts,

I am a little confused with the naming of the RTDs, 

S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 4.0.0 P19

S32K3_S32M27x Real-Time Drivers ASR R21-11 Version 4.0.0 P12

S32K3_S32M27x Real-Time Drivers AUTOSAR R21-11 Version 4.0.0 HF01

S32K388 Real-Time Drivers Version 4.0.0 CD01
Seems P = Patch, HF = Hot Fix, CD = Code Drop, then what's the difference between P/HF/CD? 
the newest RTD should be P , HF, or CD? 

Thanks

0 件の賞賛
返信
1 返信

911件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes it is:

P- Patch - comes with full RTD package as it is a release

HF - Only the fixed modules as it is not a release

CD - Code drop  - All software included in this release has Code Drop quality status in terms of testing and of quality documentation. Code Drop qualified releases are not fully tested and contain partial feature set. It is not intended to be used in production.

Always refer to the release notes of that particular package. There is a detailed description.

Best regards,

Peter

0 件の賞賛
返信