RTD 3.0.0 example code does not compile

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RTD 3.0.0 example code does not compile

157 次查看
durga_choudhury
Contributor III

I had asked a similar question before; this is different (but somewhat related).

IDE details:

S32 Design Studio for S32 Platform

Version: 3.6.2

Build id: 250529 (Update 2)

 

SDK details:

 

durga_choudhury_0-1759865678244.png

 

 

The code generator creates files in the 'board' subdirectory of the project that seem to be neither needed nor does it compile. This can be made to happen in several different ways, but one step-by-step instruction to reproduce is as follows:

 

1. Create a new project from examples.

2. Choose Adc_example_S32K148 (This happens in other examples or my own code also when a port is not configured)

3. Double click on the .mex file. It will ask you to upgrade it to the latest IDE.

4. Upgrade it and click on 'Update code'.

5. The generated code does not build because of this line in board/Port_Ci_Port_Ip_Cfg.h:

#include "Port_Ci_Port_Ip_Types.h"

which does not exist

6. Delete both board/Port_Ci_Port_Ip_Cfg.c and board/Port_Ci_Port_Ip_Cfg.h. The project will now compile.

 

Am I doing something wrong or is this an issue with the IDE?

 

标记 (2)
0 项奖励
回复
4 回复数

129 次查看
durga_choudhury
Contributor III

Hello @_Leo_ 

 

Thank you for your support. The 'Installation Details' window has 5 tabs. I suppose you wanted only the 'Configurations' tab, which I am attaching as a text file. Please let me know if I can provide any other information.

 

Best

Durga

0 项奖励
回复

91 次查看
_Leo_
NXP TechSupport
NXP TechSupport

I refer to an screenshot like the following. I could be an scrolled capture o multiple captures to see all the installation details please.

_Leo__0-1759951468382.png

 

0 项奖励
回复

86 次查看
durga_choudhury
Contributor III

Hello @_Leo_ 

 

Thank you for your support. Please find two screen shots attached. There are a significant amount of overlap between the two; one is a fully scrolled up view and the other is a fully scrolled down view.

0 项奖励
回复

134 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Thank you for your interest in our products and for contributing to our community.

Following your step-by-step instructions, after step 4 I built the project successfully:

_Leo__0-1759878903039.png

Maybe we need to take a step back and check the installation.

Please an screenshot of your "Installation Details", which you can find in "Help" tab of the IDE.

0 项奖励
回复