RD772BJBTPL8EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RD772BJBTPL8EVB

1,141 Views
Shivanand
Contributor II

Hi, im using RDK-358BMU , i want to read gpio1 from BJB using AFE1, but Measurement is possible only with AFE2, how can i do it?

Shivanand_0-1743062503592.png

 

0 Kudos
Reply
3 Replies

1,026 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Sorry for the delay in replying, 

Could u share the full system setup information:

  • The bjb is 800v bjb or 400vbjb or their own built pcb adoption of 772c bjb
  • Please refer to the hvbms integration example there we have a function for reading the bjb measurements.
  • Could you please share the code /project to actually understand the context better.
0 Kudos
Reply

978 Views
Shivanand
Contributor II

Hi @ErikaC

The BJB is 800 V.

This is the project I'm using, the HVBMS integration project, but I'm unable to get the data of the GPIO. 

0 Kudos
Reply

1,085 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

I am working on this, I will keep you informed.

0 Kudos
Reply