RD-HVBMSCTBUN, Please tell me how to build the example (S32K DS Installation)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RD-HVBMSCTBUN, Please tell me how to build the example (S32K DS Installation)

Jump to solution
1,596 Views
BAe
Contributor I

I purchased the RD-HVBMS Bundle and installed S32K DS According to the "BMS Software Installation Guide (rev2.0)" to build the examples.

Import example code and  use "Update Code" command, but there are still 5 errors.

How can I fix it?

 

S32K Version details are as follow image

BAe_0-1707886614036.png

The installation details are as follow image, It's only about SDK

BAe_1-1707886674596.png

Error details are as follow Image

BAe_2-1707886763392.png

 

0 Kudos
Reply
1 Solution
1,531 Views
adijoshi9
NXP Employee
NXP Employee

 Sorry for the confusion i missed you latest screenshot showing all the installed packages, please ignore my last message.

  1. Could you restart S32 Ds
  2. Open a new workspace and  reimport project--> build

View solution in original post

0 Kudos
Reply
11 Replies
1,551 Views
adijoshi9
NXP Employee
NXP Employee

Hi,

Have  you installed  the FS26 sbc package  in s32ds?

0 Kudos
Reply
1,548 Views
BAe
Contributor I

After installation, the result is as follows.

BAe_0-1707980514704.png

BAe_1-1707980578488.png

More bugs occur and build stops midway.

 

 

0 Kudos
Reply
1,544 Views
adijoshi9
NXP Employee
NXP Employee

As mentioned in the SW installation and user guide did follow the steps as i could see from the screenshot that some packages are missing

adijoshi9_0-1707981639071.png

 

0 Kudos
Reply
1,539 Views
BAe
Contributor I

As mentioned, the picture above is only for the SDK. (Filter applied)

It's the same as you without any filters applied.

BAe_0-1707982470152.png

 

 

0 Kudos
Reply
1,541 Views
adijoshi9
NXP Employee
NXP Employee

Do you have access to the SW installation and user guide? If not then PFB attached

0 Kudos
Reply
1,538 Views
BAe
Contributor I

As mentioned above, I did Installation According to the "BMS Software Installation Guide (rev2.0)",  the document you send.

and What is "PFB", Could you tell me?

0 Kudos
Reply
1,534 Views
adijoshi9
NXP Employee
NXP Employee

PFB is "please find below"

As I could see that the s32xx development  packages , s32k3 platform  package and s32k3 platform  tools package are missing in your s32ds?

I recommend  you to do a fresh installation,  and  follow the sequence  of installation  of the packages  mentioned  in the installation  guide.

0 Kudos
Reply
1,532 Views
adijoshi9
NXP Employee
NXP Employee

 Sorry for the confusion i missed you latest screenshot showing all the installed packages, please ignore my last message.

  1. Could you restart S32 Ds
  2. Open a new workspace and  reimport project--> build
0 Kudos
Reply
1,528 Views
BAe
Contributor I

This was resolved once and for all with the "reimport project".

Thank you so much for your help.

0 Kudos
Reply
1,573 Views
adijoshi9
NXP Employee
NXP Employee

@TomasVaverka 

Which hvbms bundle  does the customer  have 400v (775,772) ,400v(774,772)?

As the customer  has opened  hvbms Integration proj for 400v (775,772)....

 

0 Kudos
Reply
1,557 Views
BAe
Contributor I

Which hvbms bundle  does the customer  have 400v (775,772) ,400v(774,772)?

-> RD-HVBMSCTBUN (S32K344 / MC33775A)

 

As the customer  has opened  hvbms Integration proj for 400v (775,772)....

 -> The last image above shows that the project was opened but the build failed.

 

 

0 Kudos
Reply