Questions about the use of the SCST library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Questions about the use of the SCST library

跳至解决方案
4,087 次查看
Derrick_Nexus
Contributor II

Hi,NXP community:

   I want to add SCST kernel self-test code for kernel detection when using S32K146, now using IDE S32DS, when using API to call the test function found that m4_scst_exception_hard_fault1 in the test occurred an exception leading to program stuck. May I ask how to configure and use this SCST self-test library in the project? Is there something wrong with my configuration? debug check in m4_scst_exception_hard_fault1 runtime will always trigger jump to m4_scst_ISR_dispatcher, please help me find the reason, configuration is as follows:

0 项奖励
回复
1 解答
4,043 次查看
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

This description looks like an issue with connected debugger which most probably stops SCST tests execution.

In case of the debugger is connected then exceptions triggered by SCST Library for testing purposes can be captured directly by the debugger, tests execution then stop in the m4_scst_ISR_dispatcher function.

To avoid this behavior, please configure your debugger not to capture exceptions!

 

E.g. for Lauterbach debugger this can be done by running the following commands:

TrOnchip.Set.HARDERR OFF

TrOnchip.Set.BUSERR OFF

TrOnchip.Set.CHKERR OFF

TrOnchip.Set.MMERR OFF

TrOnchip.Set.STATERR OFF

 

Hope this helps…

在原帖中查看解决方案

1 回复
4,044 次查看
martinkaspar-r3
NXP Employee
NXP Employee

Hello,

This description looks like an issue with connected debugger which most probably stops SCST tests execution.

In case of the debugger is connected then exceptions triggered by SCST Library for testing purposes can be captured directly by the debugger, tests execution then stop in the m4_scst_ISR_dispatcher function.

To avoid this behavior, please configure your debugger not to capture exceptions!

 

E.g. for Lauterbach debugger this can be done by running the following commands:

TrOnchip.Set.HARDERR OFF

TrOnchip.Set.BUSERR OFF

TrOnchip.Set.CHKERR OFF

TrOnchip.Set.MMERR OFF

TrOnchip.Set.STATERR OFF

 

Hope this helps…