I want to know S32K1xx LIN Send Header, the principle of send PID?
I found below function will sent PID: LIN_LPUART_DRV_ProcessFrameHeader(**) which local in function LIN_LPUART_DRV_ProcessFrame(***) ,this function is only called in LIN IRQ function:LIN_LPUART_DRV_IRQHandler(***),detail code is:
if (***) statement is true only if the LPUART_RX_DATA_REG_FULL flag is set, but why this flag can be set when Master sent sync field successed . Did the Slave send data to the master at this time(Master sent sync field successed)? otherwise,I think LPUART_RX_DATA_REG_FULL can not be set automatically。
Hello longsheng liao,
Because the LPUART_TX/RX connect to LIN transceiver, every signal send in TX pin will be appear in RX pin. So LPUART_RX_DATA_REG_FULL will be set after master send SYNC.
Best regards,
Hung.