Dear NXP Engineer:
I have a problem when i read the expoler project like flash_partitioning_s32k144,it will meet some register,like this picture show.
and when i press ‘F3’ it will jump to definition at line 211 of file flash_driver.h. but it display it equal the “FTFC->FCNFG” .But Actually i want to know the init value about FTFx_FCNFG.If i not clear the value about it, i do not understand how to Perform '&' calculations.
So can you tell me,where are the define with the init value with this kind of register. Such as, doc name:S32SDK_S32K144_UserManual(i can't find it in this doc).and i need it download link.
And i have another question,
the problem is in lin 11226,FCFG1 init valut is that 0x4c?I can't find instances of offset,what about offsetf mean?
About first problem i found it on S32K-RM.the Reset value is 02h.the other one are solution too it value is '0',also in S32K-RM.