Program a S32K from a 820A via SWD?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program a S32K from a 820A via SWD?

920 Views
perig_vennetier
Contributor I

Hello,

I'd like to setup an embedded system to be able to have a Snapdragon 820A program a S32K144 via SWD but it seems that 820A does not support SWD natively.

Anybody would have seen a solution to do the above?

Would there be a chip that can be the bridge between SPI and SWD for example?

Could any GPIO be used on the 820A to become a SWD channel by creating custom timing?

Thanks!

Labels (1)
0 Kudos
Reply
0 Replies