Problem setting up Trace and ethernet pins in S32K148 ( ETM )

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem setting up Trace and ethernet pins in S32K148 ( ETM )

1,790 次查看
naderkhamess
Contributor III

I would like to set up the TPIU pins for trace but i have a problem that the pin PTD11 for Trace Data out 2 is already configured by ENET RMII Transmit Clock.   ( PTC2 pin is also set up for RMII Transmit data 0)

Possible solutions are: either to use less data bits but then its likely/chance to lose data, or i can make both pins available in the PCB and only when programming ENET, i will use less trace data pins.

Any other solution to be able to trace ENET with all the trace 4 data pins ? 

thanks!

Cheers,

Nader

2 回复数

1,696 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello Nader,

Unfortunately, I don't see any other solution, all the pin functions can't be used at at the same time.

BR, Daniel 

1,697 次查看
naderkhamess
Contributor III

Hallo Daniel,

Ok thanks for the answer.

BR, Nader

0 项奖励
回复