Possible to Erase/Sanitize all memory while running?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Possible to Erase/Sanitize all memory while running?

742件の閲覧回数
m_mishrikey
Contributor III

We are using an S32K148, and our customer has a requirement that the device be able to sanitize all volatile and non-volatile memory upon command, while in operation (no debugger or programmer, should wipe itself).

Is there a way to do this without a bootloader?  We presently do not have a bootloader, and using one would add significant complexity.

 

0 件の賞賛
返信
2 返答(返信)

701件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @m_mishrikey,

Volatile memories are reinitialized after every reset.

Non-volatile memories can be erased by sectors from the FTFC controller.

Except for the EEE backup. The FlexNVM should be pertitioned only once in the life time of the device.

I'm not sure I understand this use case, can you eleborate on the description?

 

Regards,

Daniel

 

0 件の賞賛
返信

697件の閲覧回数
m_mishrikey
Contributor III

I think it's either trade secret protection,  or an extreme cybersecurity requirement.   Like in the TV cartoon Inspector Gadget - "This message will self destruct in 5 seconds..."

 

 

0 件の賞賛
返信