Pin defition of ISELED_ADK_EXT_D

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Pin defition of ISELED_ADK_EXT_D

458 次查看
rockchenatpmg2020
Contributor I

There is no pin definition of ISELED_ADK_EXT_D, which is produced by dominant for ISELED ADK. 

any 8 pin defition doc.? 

thanks. 

0 项奖励
回复
2 回复数

443 次查看
rockchenatpmg2020
Contributor I

hello Robin,

this is what i need; 

the connector pin assignment is not included in UM_ISELED_ADK_rev0.8.pdf, but included in your rev0.9.pdf. 

thanks a lot.

0 项奖励
回复

445 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Do you mean "Figure 2 - Connector pin assignment topview master side" and "Figure 3 - Connector pin assignment topview slave side" in Inova ISELED ADK User Manual?

Figure 2 - Connector pin assignment topview master side.png

These schematics of the strip/adapter board have to be requested to the Inova Semiconductors team. Please contact their sales/FAEs team to get access to this.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复