Output Current S32K144-EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Output Current S32K144-EVB

2,534 Views
asrikrishnagovind
Contributor II

Hello, I have a Motor Drive application, which utilizes 4 Hall Effect Sensors (5v)  to measure phase currents, and each of the sensor requires about 20mA of current typically to operate, along with an Encoder with similar requirements.

In the Datasheet of S32K1XX: S32K1XX: S32K1xx Data Sheet (nxp.com) Page 31, it was shown that the "Output high current total for all ports is 100mA". My query is, will the Evaluation Board S32K144-EVB be able to provide the current requirements of these sensors? Thanks and Regards

Tags (1)
0 Kudos
Reply
3 Replies

2,517 Views
asrikrishnagovind
Contributor II

Thanks for the reply. Will a given GPIO port be able to source the required 20mA? I understand that collectively all the ports can source 100mA. Is there an individual pin's maximum rating due to hardware or packaging constraint? Thanks and Regards

0 Kudos
Reply

2,514 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Normal GPIOs can source 5mA at max voltage drop VDD - 0.8V at the output pin.

GPIO-HD pins (if DSE = 1) can source 20mA at max drop of 0.8V.

danielmartynek_0-1649157796494.png

In other words, if the load is 20mA per pin / sensor, the sensor will not be powered by 5V but by >= 4.2V.

The sensors can be powered from the 5V generated by the SBC directly.

 

Regards,

Daniel

0 Kudos
Reply

2,520 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @asrikrishnagovind,

The MCU can provide combined 100mA at GPIOs (Output HIGH) as you mentioned.

But the MCU is powered by the SBC UJA1169

danielmartynek_0-1649155600400.png

https://www.nxp.com/docs/en/data-sheet/UJA1169.pdf

danielmartynek_1-1649155723671.png

 

 

Regards,

Daniel

0 Kudos
Reply