OTA using UDS over the CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTA using UDS over the CAN

14,361 Views
Dileep1441
Contributor I

Hi,

There is a requirement of OTA using UDS over the CAN Commination in my project.

If there is any possibility for this requirement please share the details and process also please provide the example code.

 

Device: S32K144EVB evaluation board.

S32DS: S32 Design Studio for ARM--Version: 2018.R1

 

Thanks in advance.

0 Kudos
Reply
23 Replies

3,707 Views
Dileep1441
Contributor I

Hi @danielmartynek,

I didn't installed SDK RTM 2.0.0, could you please share the required all software and packages links,

My requirement is to run the UDS in S32K144EVB.

 

I have the below software and hardware

Device: S32K144EVB evaluation board.

S32DS: S32 Design Studio for ARM--Version: 2018.R1

0 Kudos
Reply

2,713 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Dileep1441,

The SDK package can be downloaded here:

https://www.nxp.com/design/software/development-software/s32-sdk/s32-software-development-kit-for-s3...

danielmartynek_0-1683809875291.png

danielmartynek_2-1683810564523.png

I believe this is all that is needed,

 

BR, Daniel

 

 

0 Kudos
Reply

780 Views
Dileep1441
Contributor I

Hi @danielmartynek,

Installed S32 SDK for S32K1xx RTM 4.0.3 and please share the further steps to run the UDS example project S32K144_CAN_bootloader.

after installation of the S32 SDK for S32K1xx RTM i'm trying to import the below path example project D:\unified_bootloader_demo_V2.1\unified_bootloader_demo_v2.1\S32K1xx\S32K144_CAN\S32K144_CAN_bootloader  to this S32DS Software workspace S32 Design Studio for ARM--Version: 2018.R1

also try to given the SDK path but again getting the error(PFA for the Screenshot)

 

but observed the same issue which i shared the screenshots on previous conversation.

Please guide me to run the example UDS project in S32K144EVB.

Thanks in advance.

0 Kudos
Reply