Not able to attach Autosar SDK on S32 Design Studio for S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to attach Autosar SDK on S32 Design Studio for S32K144

Jump to solution
196 Views
Kunal_Gettobyte
Contributor III

I am creating a new project on S32K144 Microcontroller using S32 Design Studio and want to use Autosar MCAL Stack.

But when i am creating new project from scratch, i am not able to add Autosaur RTD Files/stack. They are not visible in SDK list. What could be problem? How to create a new scratch project using Autosaur RTD for S32K1xx Microcontrollers.

 

WhatsApp Image 2024-06-04 at 18.01.04.jpeg

 

Even though Autosaur RTD i have downloaded and i can open its examples too. But not able to add its SDK when creating a project from scratch for S32K1xx MCU. 

WhatsApp Image 2024-06-04 at 17.59.59.jpeg

0 Kudos
Reply
1 Solution
116 Views
Kunal_Gettobyte
Contributor III

Well, its not like that.

Issue is solved. Selecting the correct compiler version while creating a project. Previously i was selecting GCC compiler 6.2, in which Autosar SDK is not showing. But by selecting GCC compiler 9.2, Autosar SDK starts showing and am able to create projects.

 

I guess Autosar RTD stack is compiler dependent.

 

Anyway thanks

Kunal_Gettobyte_0-1718133841919.png

 

View solution in original post

0 Kudos
Reply
2 Replies
117 Views
Kunal_Gettobyte
Contributor III

Well, its not like that.

Issue is solved. Selecting the correct compiler version while creating a project. Previously i was selecting GCC compiler 6.2, in which Autosar SDK is not showing. But by selecting GCC compiler 9.2, Autosar SDK starts showing and am able to create projects.

 

I guess Autosar RTD stack is compiler dependent.

 

Anyway thanks

Kunal_Gettobyte_0-1718133841919.png

 

0 Kudos
Reply
162 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Kunal_Gettobyte 

According to the information provided looks like you are using S32 Design Studio 3.4, but the S32K1_S32M24X Real Time Drivers AUTOSAR 4.4 & R21-11 Version 2.0.0 is delivered as an Update Site for S32 Design Studio 3.5. So its functionality and compatibility are not guaranteed for other IDE versions. 

 

B.R.

VaneB

0 Kudos
Reply